Is EMC plate included in Altivar ATV320 variable speed drive delivery?
Yes, the EMC plate is delivered together with the Altivar ATV320, but it is not mounted on the drive. The screws for the EMC plate installation are also included in the Altivar package.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: