How can I download firewall policies through FTP?
Issue:
How to download firewall policies over FTP

Product Line:
AP9630/31/35
Units that use an embedded NMC2 (including, but not limited to AP44xx ATS, AP8xxx PDU)

Environment:
Firmware revision v6.x and greater

Resolution:

After initiating a command line FTP session to the device, the directory will need to be changed to the "fwl" folder where the policies are saved. Please see the below picture for more information:

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: