What are the companies manufacturers or suppliers of PM8000 series meters Digital and Analog Input/Output, and Remote Display?
Issue
The McCain Law (NDAA 2019) Section 889, restricted to import the telecommunications equipment or services from certain Chinese manufacturers or suppliers.

Product Line
PM8000 series meters,

Environment
PowerLogic meters, ION meters, and Communication module.

Cause
Do the following PM8000 series meters parts; the digital input/ output METSEPM89M2600, the analog input/ output METSEPM89M0024, and the remote display METSEPM89RD96
were smart parts or/and made by the banned Chinese suppliers listed in McCain Law (NDAA 2019 Section 889)?

Resolution
The McCain Law (NDAA 2019) Section 889 on “Prohibition on certain telecommunications and video surveillance services or equipment” that can be found here on page 282. The parts concerned in this request, are the accessories of the PM8000 series meters made in China; please see the following article FA209186 for Powerlogic and ION meters country of origin.

The following table provides the information about  the parts and their suppliers:
Device TypeCommercial ReferenceComponent TypeManufacturer or Supplier

Digital Input /Output

METSEPM89M2600
MicroprocessorST Microelectronics
Driver/Receiver/TransmitterAnalog Devices /Texas Instruments
EEPROMST Microelectronic /Atmel /Microchip Technology

Analog Input /Output

METSEPM89M0024
MicroprocessorST Microelectronics
EEPROMST Microelectronics /Atmel /Microchip Technology
Digital to Analog ConverterAnalog Devices

Remote Display

METSEPM89RD96
MicroprocessorTexas Instruments
SDRAMMicron Technology /ISSI
Flash MemoryMicron Technology
Ethernet TransceiverMicrochip Technology

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: