SRT Smart-UPS reports “Battery pack x disconnected / cleared” in the NMC event log

Article available in these languages: Russisk

Issue:

SRT Smart-UPS reports “Battery pack x disconnected / cleared” in the NMC event log, with a logging interval of 17 seconds

Product Line:

Smart-UPS SRT

Resolution:

Ensure the External Battery Pack cable is securely connected, if applicable. For SRT 8 & 10kVA models, ensure both the External Battery Pack power and communication cables are securely connected. Perform a self-test with at least 500W load. If the issue persists, perform a UPS firmware upgrade to the latest firmware revision available in FA279197 .

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: