How to keep existing IP54 protection on Altivar ATV650 or Altivar ATV950 if keypad VW3A1111 is removed from Altivar?
In order to keep IP protection on the drive after the keypad has been removed, it is necessary to use blank cover VW3A1116.
Attached pdf shows the details.

Schneider Electric Danmark

Bilag
ATV_IS_IP55_Blanking_Cap VW3A1116_NVE77178_00.pdf [1.92 MB]
Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: