How does the 9050JCK16 On Delay timer work?
Issue:
Installation and wiring for the 9050JCK1* On Delay timers.

Product line:
9050 Type JCK timer

Environment:
Adjustable On Delay timers

Cause:
No trigger contact for the timer function

Resolution:
There is no trigger contact with the 9050JCK1* On Delay timers.  The timing function for on delay begins with the coil voltage being applied.  When the coil voltage is applied the timing period begins.  At the end of the timing period, the contacts will change state.

To reset the timer, remove the coil voltage.

Schneider Electric Danmark

Bilag
9050JCK1(x) On Delay timer.JPG.jpg [52.49 KB]
9050JCK1(x) On Delay timer wiring.JPG.jpg [24.74 KB]
Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: