What is the first official commercialized firmware version for 140CRA31200?
Issue
The 140CRA31200 is an adapter module on a Quantum remote I/O drop and customers would like to knwo what is the firmware history including the first official commercialized version.

Product Line
M580, Quantum, Quantum ERIO

Environment
140CRA31200

Resolution
The first official commercialized firmware version is 1.09 and the spreadsheet below shows the official firmware versions until 7/2019. All the firmware versions older than 1.09 are Schneider Electric internal versions from Field Tests modules and cannot be used by customers.
Firmware versionDescription
1.09First official commercialized version
2.14First enhancement firmware (support of M580 HSBY)
2.30Second enhancement firmware (04/2018)
2.40Latest enhancement firmware (02/19)

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: