Quick Access Toolbar is Hidden in Secondary Window Container
The QAT (Quick Access Toolbar) feature for secondary window containers which allows database items such as Mimics, Lists, Trends or reports to appear simultaneously on separate monitors has been removed from latest releases of ClearSCADA as part of secondary window container improvements as shown below. The change was made back in ClearSCADA 2017 and ClearSCADA 2015 R2 August 2017 Update. This means that all versions of ClearSCADA 2017 R2 and R3 had the same improvement in them.


Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: