What's the correct torque for the screws on the NetShelter SX vertical mounting rails and accessory rails?
Issue:
Torque for the screws is not noted in the manual.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:

Torque is needed to properly tighten the mounting rails or accessory rails after they're moved.

Resolution:

Torque Specs: 32-48 IN-LBS

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: