How to monitor RAM battery voltage on RemoteConnect?
To monitor the RAM battery voltage, use System Analog Point ‘SYS_INFO_MemoryBatteryVoltage’ that point will indicate the device battery voltage in real format.

Another way to indicate low battery is alarm using below system points,
  • SYS_INFO_NVretentionAlert with data type ‘Digital’ used with firmware 9.1.1 or earlier only
False = Normal
True = Alert (Lithium battery low)
  • SYS_INFO_MemoryBatteryAlert with data type ‘Digital’ used with firmware 9.1.2 or later only
False = Normal
True = Alert (Lithium battery low)

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: