NetBotz 700 Series | Supported Cameras
Issue:
Supported Cameras for the NetBotz 700 Series Appliances

Product Line:
NetBotz Rack Monitor 700 Series
- NetBotz Rack Monitor 750 (NBRK0750)
- NetBotz Wall Monitor 755 (NBWL0755/NBWL0756)

Environment:
NetBotz Rack Monitor 700 Series
NetBotz 700 Series Cameras

Resolution:

Supported Cameras are the NetBotz Camera POD 165 (NBPD0165) and ONVIF Profile S Cameras.
NOTE: Motion Detection and other features may be limited when using non-NetBotz ONVIF cameras. Learn more at www.onvif.org

Schneider Electric Danmark

Se mere
Produkt:
Område:
Artikler som kan være nyttige
Se mere
Produkt:
Område: