Are the NetShelter VX Seismic cabinets and 2-Post Racks OSHPD compliant?
Issue:
the question has been risen if a NetShelter VX Seismic cabinet is OSHPD compliant.

Product Line:
NetShelter VX Seismic, 2-Post Rack

Environment:
AR2144BLK, AR2145BLK, AR201: all serial ranges.

Cause:
The only seismic documents on the product pages of AR2144BLK and AR2145BLK are the NEBS GR-63-CORE Zone 4.
There are no seismic documents on the product page of AR201.

Resolution:

Several Smart-UPS were tested and approved for installation with NetShelter VX Seismic and AR201 during OSHPD Special Seismic Preapproval (OSP) testing. Please see the attachment.

Schneider Electric Danmark

Bilag
OSHPD OSP 2016.pdf [3.27 MB]
Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: