PME 9.0 - Dial real time objects do not display properly in Vista when some Regional formats are used
Issue
Dial real time objects do not display properly in Vista when some Regional formats are used

Product Line
Power Monitoring Expert 9.0

Envoriment
Vista - Diagrams

Cause
This will happen if the decimal separator for the region setting is "," rather than ".".

Resolution
This solution is exclusively for PME 9.0

1) Apply CU2 - This MUST to be done before applying the solution
2) Shut down all Vista instances
3) Backup the existing vista.exe - it's in the PME\system\bin folder just in case
4) Replace it with the attached updated version of vista.exe
5) This should be done on the Application server and all Engineering Clients.

Schneider Electric Danmark

Bilag
vista.exe [3.93 MB]
Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: