PME - RAM and CPU usage are high, but PME is not logging new data

Issue

RAM and CPU usage are high, but PME is not logging new data

Product line
Power Monitoring Expert 9.0

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Environment

Microsoft Windows 10


Cause
"ION Log Subsystem Router Service" runs the stored procedure “RebuildAlarmRelatedIndexes” to rebuild indexes on major ION_DATA tables.
For large databases, it may take longer and affect system performance.

Resolution
Update the stored procedure to do a REORGANIZE vs a REBUILD function on the indexes.
The attached SQL file will make the required changes in the "RebuildAlarmRelatedIndexes" stored procedure.



Schneider Electric Danmark

Bilag
RebuildAlarmRelatedIndexes_modification.sql [808 Bytes]
Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: