What are the replacement screws for Model 6 Motor Control Center Side (End) Plates
To order the proper replacement screws a couple of things must be known.
1.) Enclosure type
2.) Non-Arc Resistant or Arc Resistant Enclosure.
Based on the criteria above the part numbers below can be ordered.

M6 MCC Non-Arc Resistant (Standard):
Enclosure Type: 1 or 1A
  • Part Number: 21427-17121
  • Qty(12) typically required
Enclosure Type 12
  • Part Number: 80450-225-01
  • Qty (12) typically required
M6 MCC Arc Resistant:
Enclosure Type 1 or 1A
  • Part Number: 21490-17161
  • Qty (31) typically required
Enclosure Type 12
  • Part Number: 80450-225-01
  • Qty (31) typically required

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: