Scadapack Workbench CAM3 Simulator problem
To resolve this issue running Scadapack Workbench CAM3 Simulator.

Actions:
Change ISA11 security settings according the release notes  --> change R/W access on ISA11 for all users.
Please check if you have a file on simulator .ini file so change to Everyone can edit it.

From Release Notes SCADAPACK
  • To enable simulating CAM 3 projects, you need to run the Workbench with administrator privileges: [9294]
    • From the Start menu, locate and right-click the ISaGRAF Workbench, and then click Run as administrator.
· On Windows 2000, they're called a "Restricted User" account.
· On Windows XP, they're called a "Limited" account.
· On Windows Vista, they're called a "Standard User" account.
· On Windows 7, User Account Control (UAC)

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: