What is the difference between iEM3455 and iEM3455C1/C2 models?
Issue

Value of CT primary cannot be changed in iEM3455C1 and iEM3455C2 models

Product line

Powerlogic Meter iEM3000 series

Environment

Front panel
ION Setup 3.2

Resolution

The difference between the models iEM3455, iEM3455C1 and iEM3455C2 are that of CT primary configuration. For iEM3455, CT primary can be changed to any LVCT but the value in iEM3455C1 and iEM3455C2 is fixed to 100 amps and 200 amps respectively, this cannot be modified.

iEM3000 series documentation can be found at the following link FA352325

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: