What is the time limit for BMX Analog inputs to withstand their specified isolation voltage values?
Issue
The isolation voltage specifications for BMX Analog inputs do not specify a time limit.  What is the time limit for the isolation voltage specifications?

Isolation voltage example for a BMXAMI0810



Product Line
x80 Analog inputs


Resolution
There is no isolation voltage time limit.  The module can withstand the maximum isolation voltage indefinitely without any damage.


Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: