Power Monitoring Expert - Vista View Only login does not work
Issue
Cannot log into Vista using the "View Only" option.
It gives an error message:




Product Line
Power Monitoring Expert 2020
Power Monitoring Expert 9.0

Environment
Vista login

Cause
For security reasons, using "View Only" button to log into Vista no longer works and will cause an error message to display.

Resolution
It is recommended to log into the Diagrams Web Application with an Observer-level user instead.

Additional Notes
A note related to this behaviour will be included in the next release of the System Guide 2021.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: