What are the maximum Session/Subscription for the BMENUA0100 with the firmware version 1.01.50?
1.    Issue
Client wants to know what are the maximum Session/Subscription for the BMENUA0100 ?

2.    Product Line
Firmware version 1.01.50

3.    Environment
BMENUA0100

4.    Resolution

Here you are the limitation Session/Subscription for the BMENUA0100

The maximum session to be open is 3.
The maximum subscription to be open per session is 4.

Total subscription is 12.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: