How to create an alarm filter for instances of a template in Geo SCADA
Problem:

I have multiple instances of a template. Each instance represents an area and has a mimic with an embedded alarm list. The embedded alarm list for each instance needs to show alarms specific to this particular instance. How can this be done?

Solution:

Consider setting up an expression in the Embedded List's animations in the template itself. The expression could, but does not have to, be similar to the one below:

Animated property: Filter
Animation expression: 'Source="'+".FullName"+'.*"'

The above expression will allow the list to display alarms from all sources (objects) whose full names start with the name of each particular instance.


Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: