Where is the KLC output filter mounted relative to the drive and the motor?
Issue:
KLC output filter mounting relative to the drive and the motor

Product Line:
Altivar Drives

Environment:
All

Cause:
N/A

Resolution:
KLC filters are designed to be located immediately adjacent to the output terminals of the drive and to be wired directly to the drive output. The distance from the drive outputs to the filter inputs should be as short as practical.

Schneider Electric Danmark

Se mere
Kategori:
Artikler som kan være nyttige
Se mere
Kategori: