Søg i ofte stillede spørgsmål
How many numbers of channels supported by BMENOR2200H in the IEC104 Server Configuration?
The BMENOR2200H supports a maximum of 4 channels when configured as IEC104 server configuration.
Note:
Note:
- There is one main channel and the rest 3 of them are the virtual image of the main channel.
- The events in all 4 channels are not synchronized among them. Duplicated across all 4 channels
- To avoid the duplicated events the BMENOR2200H supports the IEC104 Server channel redundancy feature.
Udgivet til:Schneider Electric Danmark
Se mere
Produkt:
Se mere
Produkt: