What is the Bridge Priority for RSTP in HEP meters

Issue
RSTP bridge priority cannot be configured on HEP meter that supports RSTP
_____________________________________________________________

Product Line
ION9000
ION9000T
PM8000
ION7400
_____________________________________________________________

Environment
Meter Firmware
_____________________________________________________________

Solution
The RSTP bridge Priority is not a user configurable setting. The value defined in the meter's firmware is 32768.
_____________________________________________________________

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: