How to use the VW3A1111 graphic keypad to check the Drive Identification, including part number, serial number and options installed.
Issue:
Customer needs to know the Serial number of his drive, and other information like firmware version and option cards

Product Line:
ATV600, ATV900 and ATV340

Environment:
Must be using the Graphic Keypad VW3A1111

Cause:
This information may not be easily accessible if the label of the drive is hidden or blocked

Resolution:
See the attached PDF for details on how to accomplish this along with a brief description of what information is shown.

Schneider Electric Danmark

Bilag
Drive ID using VW3A1111 display.pdf [729.02 KB]
Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: