Does the BMENUA0100 have the capability of buffering or holding events/data while the comms are down?

Issue

Event buffering

Product Line

BMENUA0100

Environment

EcoStruxure Control Expert

Resolution

The NUA module does not have a buffer to hold events. If comms go down then the events will be lost. Buffering or holding events is not in the OPC UA spec.

Schneider Electric Danmark

Se mere
Produkt:
Artikler som kan være nyttige
Se mere
Produkt: