How do I change the "Installer" account password for the BMENUA0100 OPC UA module?
Issue:
How to change the password for the BMENUA0100 OPC UA module Installer account


Product Line:
BMENUA0100, EcoStruxure Control Expert

Resolution:
The installer password can be changed. However the module must be in the standard mode by setting the rotary switch located at the back of the module.  Once in standard mode, log into the module via your browser using the default user name and password. once connected, you will see "Installer" in green in the top right corner of the browser. click on it, and you will see the option to change password.
installer

Schneider Electric Danmark

Se mere
Produkt:
Artikler som kan være nyttige
Se mere
Produkt: