How do I disable the HTTPS network service of the BMENUA0100 OPC UA module?
Issue:
Disabling the HTTPS network service of the BMENUA0100 OPC UA module


Product Line:
BMENUA0100, EcoStruxure Control Expert

Resolution:
The HTTPS service of the BMENUA0100 OPC UA module can be disabled. The module must be in secure mode to disable the service. Once you are logged in, go to the "cyber security setup" tab then select "settings" then select "network services"

admin

Schneider Electric Danmark

Se mere
Produkt:
Artikler som kan være nyttige
Se mere
Produkt: