NetBotz NBWL0755: Private LAN NBPD0165 camera may intermittently lose communications with main unit
Issue:
NetBotz NBWL0755: Private LAN NBPD0165 camera may intermittently lose communications with main unit

Product Line:
NetBotz V5

Environment:
NBWL0755
NBPD0165

Cause:
An issue has been found where the private LAN camera pod NBPD0165, when powered from the NBRK0755, may intermittently lose communications with the main unit.

Resolution:
Please contact your local tech support with the serial number of the unit(s). In some instances, connecting a special USB dongle may be necessary to prevent this issue from reoccurring.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: