When my SoMachine v4.3 project is built, there is a version mismatch of the GMC Independent Base Device 1.2.9.0 Library
Issue
When my SoMachine v4.3 project is built, there is a version mismatch of the "GMC Independent Base Device, 1.2.9.0" Library. In the Library Manager, there is an yellow triangle with an exclamation mark on the Library.
GMC Independent Base Device, 1.2.9.0 Exclamation in Library Manager

The newest version of the library that comes with my PC's installation of SoMachine is "GMC Independent Base Device, 1.2.8.0".
Where do I obtain the newer version of the library?

Product Line
SoMachine v4.3

Environment
Programming software in Windows 7/10

Resolution
This GMC Independent Base Device 1.2.9.0 library is required to be used with the GMC Independent Altivar 1.1.5.0 library for Altivar Drives. It is contained in SoMachine v4.3 Patch 3.
SoMachine v4.3 Patch 3 can be obtained through the Schneider Electric Software Update Tool.

By default the Software Update tool is just named "Software Update" as a Desktop shortcut icon.

It can also be launched from (Default location):
C:\Program Files (x86)\Schneider Electric\SESU\SoftwareUpdate.exe

NOTE: SoMachine v4.3 Patch 2 must be installed first as a pre-requisite

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: