Can I obtain the MAC address of my TM221 controller while online ?
Issue:
Obtaining the MAC address of the TM221 controller while online


Product Line:
Ecostruxure Machine Expert Basic, TM221


Resolution:
Yes, The MAC address of the TM221 is located in system words %SW107 to %SW109.
image1

Schneider Electric Danmark

Se mere
Produkt:
Artikler som kan være nyttige
Se mere
Produkt: