License Manager returns error 'Value Cannot be Null'.

Control Expert fails to open after installing Machine Expert.  Attempts to open the License manager returns the error 'Value cannot be Null'.
error



The following steps can be used to resolve the issue.


1) Uninstall the License Manager version 2.8.2

2) Reboot the PC.

3) Re-install License Manager 2.8.1 (See attachment)


Schneider Electric Danmark

Bilag
setup_Schneider_Electric_License_Manager_sfx_V2.8.1.0.exe [138.24 MB]
Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: