Does Vijeo Designer support Harmony P6?
Harmony P6 is a new iPC range and it is supported by Vijeo Designer as a Harmony iPC from the version VJD 6.2 SP12.
The goal of this article is to inform about registration policy and the target model.

This article is applicable to the following products:
Harmony P6

This topic is related to Vijeo Designer and Vijeo Designer Runtime for Windows

The Harmony P6 has been tested and validated with Vijeo Designer as a Harmony iPC from the version VJD 6.2 SP12.
Below, please find the License type and the Target Model for the Harmony P6 from VJD 6.2 SP12.

The License type and the Target Model for the Harmony P6 from VJD 6.2 SP12

Schneider Electric Danmark

Se mere
Produkt:
Område:
Artikler som kan være nyttige
Se mere
Produkt:
Område: