Do the Modbus Plus MBX Drivers work on Windows 11?

Issue

Windows 11 support

Product Line

TSXCUSBMBP

Environment

Modbus Plus

Resolution

The latest MBX drivers (v9.0) will work on Windows 10 and 11. The part number for the drivers only is SWMXDS001. If you were to purchase an adapter with part number TSXCUSBMBP you would also get a copy of the drivers.

Schneider Electric Danmark

Se mere
Produkt:
Område:
Artikler som kan være nyttige
Se mere
Produkt:
Område: