Why can't I download to a brand new HMIGTO / HMIGK with Vijeo Designer 6.2 SP11 or older?
Issue:
Can't download to a new HMIGTO / HMIGK using Vijeo Designer v6.2 SP11 or older.

Product Line:
HMIGTO and HMIGK families of HMIs

Environment:
Vijeo Designer v6.2

Cause:
The new HMIGTO/HMIGK families have a hardware component change that requires Vijeo Designer v6.2 SP12.

Resolution:
The Harmony HMIGTO and HMIGK families of HMIs that are manufactured recently withSV4.0 or later on the sticker on the back of the HMI require Vijeo Designer v6.2 Service Pack 12.

Please find the download links for SP12 here:
https://www.se.com/us/en/faqs/FAQ000239885/

Schneider Electric Danmark

Se mere
Produkt:
Artikler som kan være nyttige
Se mere
Produkt: