How to update an X80 IO card in local rack using EcoStruxure Automation Device Maintenance

Product:

EcoStruxure Automation Device Maintenance (EADM)

Version:

3.1.147

Connection Method :

USB cable

1- Launch EADM

2- Manually add your CPU

Adding the CPU

Adding CPU part 2

3 - Login to the device (at least for firmware download)

Logging in the CPU for firmware access

4 - Go to "Extensions"

Extensions

5 - Manually the X80 IO card

Adding the X80 IO card

6 - The EADM tool will fetch information from that card

Fetching information

7 - Pick the firmware file to use from your database

Picking firmware

8 - Select firmware file

Picking firmware part 2

9 - Start the update

Updating

Schneider Electric Danmark

Se mere
Produkt:
Artikler som kan være nyttige
Se mere
Produkt: