Which Vijeo Designer Targets are compatible with the Siemens TIA Ethernet driver?

Issue: The Siemens TIA Ethernet driver is not showing as an option when the target HMI is set to HMIS5T.

Product Line: HMISCU, HMIGTO, HMIGTU, iPC, HMISTO5, HMISTU, HMIS5T, XBTGT

Environment: Vijeo Designer v6.2

Resolution:

The Siemens TIA Ethernet driver is supported by the following HMI families on Vijeo Designer: HMISCU, HMIGTO, HMIGTU and iPC.

The Siemens TIA Ethernet driver is NOT supported by the following HMI families: HMISTO5, HMISTU, XBTGT.

Schneider Electric Danmark

Se mere
Produkt:
Artikler som kan være nyttige
Se mere
Produkt: