How to safely distribute database folders to another disk/location in Geo SCADA/ClearSCADA.
*Warning: This article contains information about editing the registry. Improper changes to the registry can permanently damage the operating system.
Always backup the registry before making any changes.*


Sometimes there is a need to distribute your database folders to other disks or locations.
This can be achieved by using the Registry Editor method. Below is a quick run through on how this method could be used.
  1. Shut down the server from the server icon as follows.

server shut down
2. Locate the desired original folder you need to relocate in the database.
locate folder
3. Move the copied folder to the desired location.
4. Then open Registry Editor, locate the folder as follow HKEY_LOCAL_MACHINE\SOFTWARE\Schneider Electric\ClearSCADA\DB Change the location there, same as the folder you copied earlier.
registry editor
5. Start geo Scada server again and notice the location will change automatically in the server configuration.
geo scada server

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: