How to set the Ethernet transfer to always be enabled in EcoStruxure Operator Terminal Expert.

Issue:

Every time I need to transfer a new version of a project to the HMI, I have to enable the transfer via Ethernet.

Is it possible to have it permanently set to enabled?

Product Line:

EcoStruxure Operator Terminal Expert (all version)

Resolution:

The fact of always have to re-enable the Ethernet transfer method is normal for cybersecurity reason. But yes, it is possible to set it to always be enabled:

Help information

Configuration in EOTE

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: