Is the embedded NMC capable of reading or detecting the AP9613 dry contact when inserted into the Smart slot of the UPS?
Issue: Clarification about the accessory board (AP9613) and the embedded NMC

Product line: All Smart UPS with Embedded NMC and available Smart slot

Answer:
No!
The embedded NMC cannot detect or read the dry contact AP9613.

An embedded NMC as well as the removable/preinstalled NMC can only detect a dry contact which is directly connected to its I/O  port.

Embedded NMC and AP9613 Dry Contact.JPG

Schneider Electric Danmark

Se mere
Produkt:
Se mere
Produkt: