What is the part number for the flange kit for the ATV340 Drives?

Product Line:

ATV340 Drive flange kit part number.

Environment:

ATV340D30N4E thru ATV340D75N4E only

Cause:

Flange kits

Resolution:

Flange kit NSYPTDS4 will fit the

ATV340D30N4E

ATV340D37N4E

Flange kit NSYPTDS5 will fit the

ATV340D45N4E

ATV340D55N4E

ATV340D75N4E

Note you may need to remove the conduit kit at the bottom of the drive to install the flange kit.

ATV340 flange kit FAQ 1

Schneider Electric Danmark

Bilag
ATV_Flush_Mounting_Kit_IS_NSYPTDS4-S5_NHA2526101_01.pdf [19.06 MB]
Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: