How do I create a Move block in EcoStruxure Machine Expert Basic?
Issue:
How to move value from one memory word to another


Product Line:
EcoStruxure Machine Expert Basic


Resolution:
To perform a move operation, you can use the operate function block. Add the operate block to your code by clicking on the icon then drag to the end of the rung.
image1

Next enter the desired operation. in the example below, the value of %MW5 is moved to %MW1.
image2

Schneider Electric Danmark

Se mere
Produkt:
Artikler som kan være nyttige
Se mere
Produkt: