TM3BCEIP This site can't provide a secure connection ERR_SSL_VERSION_OR_CIPHER_MISMATCH

TM3BCEIP
This site can't provide a secure connection
ERR_SSL_VERSION_OR_CIPHER_MISMATCH

Edge browser > Settings > Default browser > Allow IE Mode > Add pages http://90.0.0.1/ & https://90.0.0.1/

Firmware update to v2.5.1.0

NB.

Remember to adjust IP address on RNDIS USB Ethernet on PC to 90.0.0.2

Firmware v2.5.1.0 fixed the issue, and it will be fixed out-of-box on devices marked SV 2.5

Schneider Electric Danmark

Se mere
Produkt:
Artikler som kan være nyttige
Se mere
Produkt: