Søg i ofte stillede spørgsmål
Control Expert application file type required for troubleshooting BMENOP0300 related cases.
Whenever a case is submitted for troubleshooting the BMENOP0300 IEC61850 Communications module, the exported Control Expert application in a 'xxx.sta' format must be provided. Do not use the auto generated 'xxx.auto.sta' file that is created when the 'xxx.stu' project is saved.
The reason is because only the exported 'xxx.sta' file will include the associated IEC61850 Configuration Tool project files.
The reason is because only the exported 'xxx.sta' file will include the associated IEC61850 Configuration Tool project files.
Udgivet til:Schneider Electric Danmark
Se mere
Produkt:
Se mere
Produkt: