How to upgrade your NMC2 & NMC3 firmware using the NMC Firmware Update Utility
Public

Issue:
The customer asked how to upgrade the firmware through the utility tool.

Product line:
NMC2, NMC3

Environment:
AP9630, AP9631, AP9640 & AP9641

Cause:
Web interface displays a UPS not recognize error or the customer is installing a new NMC.

Resolution:
Please follow the next steps.
1.- Download the .zip file with the firmware from the firmware link:
2.- Extract the file and run it:
firmware version(Version number as reference only)
3.- Enter the next information, Host (Ip address of the unit), UserName and Password of the NMC.
after that, click on Start Update, if you notice that the application stops with the selected protocol (SCP for this case) please try with FTP:
Firmware utility



Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: