Can Tesys Island Ethernet bus couplers be daisy chained to a Modicon PLC?

Issue

Can Tesys Island Ethernet bus couplers be daisy chained to a Modicon PLC?

Product Line

M340,M580 controllers

M221,M241,M251,M262 controllers

Tesys Island product line

Environment

EcoStruxure Machine Expert software

EcoStruxure Control Expert software

Tesys Island Ethernet bus coupler TPRBCEIP

Resolution

The answer is "Yes", a daisy chain connection can be made using the 2 communication ports of the Tesys Island.

Schneider Electric Danmark

Se mere
Produkt:
Område:
Artikler som kan være nyttige
Se mere
Produkt:
Område: