{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
RS-485 Converters for the UPS SmartSlot Building Management Card (AP9622)

Issue



RS-485 Converter Compatibility for AP9622 Building Management Modbus/JBUS UPS SmartSlot card

Product Line

  • UPS Device Management
    • AP9622 Building Management Modbus/JBUS UPS SmartSlot Card

Environment



AP9622 installations requiring RS-232 to RS-485 converter to work with various Building Management Systems

Cause



The AP9622 card supports RS-232 Modbus/JBUS output. Users may require RS-485 adapters to work with an existing Building Management System. Refer to compatibility list below.

Resolution




The Building Management Integration Card (AP9622) will work with the following RS-232 to RS-485 converters:
  • B&B Electronics P/N: 485OT9L*
*Item is currently discontinued per B&B. The recommended replacement is 4WSD9OTB but it has not been tested with the AP9622.
  • B&B Electronics P/N: 485LP9TB
Below is an example diagram for a 485LP9TB application:


Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :