{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Network Management Card Event Configuration Config.ini Syntax

Article available in these languages: Espagnol


Issue

Need assistance understanding the config.ini syntax relating to the [EventActionConfig] or [DeviceControlPolicyConfig] sections.


Product Line
  • Network Management Card 1 (NMC1) - AP9617, AP9618, AP9619
Devices with an embedded Network Management Card 1 include (but are not limited to): Metered/Switched Rack PDUs (AP78XX, AP79XX), Rack Automatic Transfer Switches (AP77XX, Environmental Monitoring Units (AP9320, AP9340, Netbotz 200)
  • Network Management Card 2 (NMC2) - AP9630/AP9630CH, AP9631/AP9631CH, AP9635/AP9635CH
Devices with an embedded Network Management Card 2 include (but are not limited to): 2G Metered/Switched Rack PDUs (AP84XX, AP86XX, AP88XX, AP89XX) manufactured prior to certain dates in 2023, Certain Audio/Video Network Management Enabled products.
  • Network Management Card 3 (NMC3) - AP9640, AP9641, AP9643
Devices with an embedded Network Management Card 3 include (but are not limited to): Metered/Switched Rack PDUs (AP84XX, AP86XX, AP88XX, AP89XX), APDU9XXX, Automatic Transfer Switches (AP44XXA)


Environment
  • All serial numbers
  • Users working with config.ini and event notifications/device control policy

Cause

The syntax is provided for general information and understanding of the config.ini sections noted.


Resolution

Refer to the attached PDF supplement.


Schneider Electric Algeria

Pièce(s) jointe(s)
NMC INI Syntax v3.pdf [92.01 KB]
En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :