Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
		
En quoi pouvons-nous vous aider aujourd'hui ?
Video: How do I configure a 208v Smart-UPS RT or SRT for use with a 240v input?

Issue:
How do I configure a 208v Smart-UPS RT or SRT for use with a 240v input?

Product Line:
Smart-UPS Online (RT and SRT)

Environment:
All models, All Serial Numbers

Cause:
Smart-UPS RT and SRT units sold in North America are factory configured for 208v in/out.

Resolution:
The Smart UPS Online line has a very broad range of acceptable input voltages, and as such you do not need to do anything on the input side. By default the unit will accept the 240v input but continue to provide 208v output.

In order to avoid a sudden voltage shift in the event that the UPS goes to bypass it is recommended to configure the UPS output to match the UPS input.

For SURT Models:
This can be done via a Hyper terminal session, or more commonly using the Network Management Card interface. Before any changes can be made, you must first turn off the UPS. From within the Network Management Card web interface you would select the UPS tab. On the UPS tab we would select Configuration and then Power. Here we choose 240 VAC output and click Apply. The UPS will now output 240v. Note: Output voltage will not change if the UPS is left "on" while trying to make the change.

For SRT Models:
This can be done using the LCD screen on the UPS or via the Network Management Card interface. Before any changes can be made, you must first turn off the output of the UPS. From the LCD screen go to the "Configuration" menu, then select "Output Setting" to adjust. Note: "Output Setting" will not appear in the menu if the UPS output is left on. From the Network Management Card interface, follow the same directions as the SURT that are listed above.

Please note that this is an unbalanced output with no neutral provided. If you need 120 v for your equipment you will still need to use a stepdown transformer.

The Stepdown Transformer must allow for 240v input, such as the SURT003 or APTF10KT01.

The AP9626, AP9627, and AP9628 would not be appropriate as they are designed for 208v input only.

The following video demonstrates how to configure the output voltage of Smart-UPS Online SRT Series via the display:

Schneider Electric Algeria

Video: How do I configure a 208v Smart-UPS RT or SRT for use with a 240v input?

Issue:
How do I configure a 208v Smart-UPS RT or SRT for use with a 240v input?    

Product Line:
Smart-UPS Online (RT and SRT)

Environment:
All models, All Serial Numbers

Cause:
Smart-UPS RT and SRT units sold in North America are factory configured for 208v in/out.

Resolution:
The Smart UPS Online line has a very broad range of acceptable input voltages, and as such you do not need to do anything on the input side. By default the unit will accept the 240v input but continue to provide 208v output.

In order to avoid a sudden voltage shift in the event that the UPS goes to bypass it is recommended to configure the UPS output to match the UPS input.

For SURT Models:
This can be done via a Hyper terminal session, or more commonly using the Network Management Card interface. Before any changes can be made, you must first turn off the UPS. From within the Network Management Card web interface you would select the UPS tab. On the UPS tab we would select Configuration and then Power. Here we choose 240 VAC output and click Apply. The UPS will now output 240v. Note: Output voltage will not change if the UPS is left "on" while trying to make the change.  

For SRT Models:
This can be done using the LCD screen on the UPS or via the Network Management Card interface. Before any changes can be made, you must first turn off the output of the UPS. From the LCD screen go to the "Configuration" menu, then select "Output Setting" to adjust. Note: "Output Setting" will not appear in the menu if the UPS output is left on. From the Network Management Card interface, follow the same directions as the SURT that are listed above.

Please note that this is an unbalanced output with no neutral provided. If you need 120 v for your equipment you will still need to use a stepdown transformer.

The Stepdown Transformer must allow for 240v input, such as the SURT003 or APTF10KT01.

The AP9626, AP9627, and AP9628 would not be appropriate as they are designed for 208v input only.

The following video demonstrates how to configure the output voltage of Smart-UPS Online SRT Series via the display:
 

Schneider Electric Algeria

En savoir plus
Gamme :
En savoir plus
Gamme :
En savoir plus
Gamme :
En savoir plus
Gamme :

Besoin d'aide ?

  • Commencez ici !

    Trouvez des réponses dès à présent Rechercher une solution par vous-même ou contacter l'un de nos experts.

  • Contactez le support

    Contactez notre équipe du service client pour obtenir plus d'informations, un support technique, une assistance en cas de plaintes, etc.

  • Où acheter ?

    Trouvez facilement le distributeur Schneider Electric local le plus proche.

  • Parcourir la FAQ

    Obtenez les réponses dont vous avez besoin en parcourant la foire aux questions (FAQ) par sujet.

  • Contacter le service commercial

    Effectuez une demande de renseignements en ligne et un expert vous contactera.

  • Documentation produit
  • Téléchargement de logiciels
  • Sélecteur de produits
  • Substitution et remplacement de produits
  • Centre d'aide et de contact
  • Trouver nos sites
  • Obtenir un devis
  • Où acheter
  • Carrières
  • Qui sommes-nous ?
  • Signaler une mauvaise conduite
  • Accessibilité
  • Partenaires
  • EcoStruxure
  • Nos emplois
  • Blog
  • Politique de confidentialité
  • Mention sur les cookies
  • Change your cookie settings
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.