When configuring external batteries with a Smart-UPS XL you must manually tell the UPS how many batteries are connected.
Product Line:
Smart-UPS XL
NOTE: This does not include "SMX" units. SMX models have smart batteries which do not require the use to manually add them.
Environment:
All XL models, All Serial Numbers
Cause:
Smart-UPS XL models do not feature communication with the battery packs.
Resolution:
When configuring external batteries with a Smart-UPS XL you must manually tell the UPS how many batteries are connected. The exception to this is the new SMT and SMX Smart-UPS which use intelligent battery packs and will auto-configure.
Each external battery pack is configured as ""1"" within Powerchute Business Edition or the Network Management card and we recommend no more than 10 battery packs connected.
The exceptions to this are:
SU48RMXLBP - Each unit counts as ""2"" in the interface. Connect a maximum of 5 of these packs.
UX or UXA Series Ultra Battery Packs - Each unit counts as ""5"" in the interface. Connect a maximum of 2 of these packs.
SURT - Depending on their firmware revision, some SURT units may count their internal battery as number 1. (IE: An SURT3000XLT + 1 External Battery would be set to 2 in Powerchute). On these units ""0"" is not an option that is available in Powerchute or the Network Management Card. If you are able to set your unit to ""0"", the first external battery would be ""1"". If you are not able to set your unit to ""0"", the first external battery would be ""2""
All other Smart-UPS count the internal battery as 0. (IE: An SUA3000XL + 1 External Battery would be set to 1)
For Information on which battery packs are compatible with your UPS or what estimated runtimes will be for your configuration, please visit the product page for you UPS at http://www.apc.com
"Publié pour: Schneider Electric Algeria
Besoin d'aide ?
Commencez ici !
Trouvez des réponses dès à présent Rechercher une solution par vous-même ou contacter l'un de nos experts.
Contactez le support
Contactez notre équipe du service client pour obtenir plus d'informations, un support technique, une assistance en cas de plaintes, etc.
Où acheter ?
Trouvez facilement le distributeur Schneider Electric local le plus proche.
Parcourir la FAQ
Obtenez les réponses dont vous avez besoin en parcourant la foire aux questions (FAQ) par sujet.
Contacter le service commercial
Effectuez une demande de renseignements en ligne et un expert vous contactera.